Dear, All
Customers are considering using ADS1220.
They want to use ANALOG INPUTS is single end.
So, the negative side becomes the voltage of AVSS.
Also, to convert plus/minus voltage signals, AVDD and AVSS use plus/minus power supply.
However, the provision of 'Recommended Operating Conditions' became a problem.
Vref = V(REFPx) - V(REFNx)
Is defined as 0.75V and the value of Max is defined as AVDD.
AVDD = +2.5V
AVSS = -2.5V
in the case of,
Vref = V(REFPx) - V(REFNx)
Is 2.5V the Max value?
Can it be used up to 5V?
Please tell me.
If it is 2.5V, they can not use it.
Thanks, Masami M.