Part Number: ADS1194
Other Parts Discussed in Thread: ADS1298
Hi,
We are trying to design a 6 leads ECG with 4 electrodes + 1 RLD electrode with your ADS1194.
In our design, we connected :
RA-LA to channel 1
RA-LL to channel 2
RA-V1 to channel 3
RLD electrode to RLD_IN, RLD_OUT. And RLD_INV through a 0.01 uF cap and a 392 kOhm resistor.
Then I set the CONFIG3 register to :1101 1100
PD_REFBUF enable
VREF 2.4V
RLD_MEAS RLD_IN routed to channel 3
RLDREF feed internally
RLD BUFFER enabled
RLD LO SENSE disabled
RLD connected
But then I still have strong common mode interferences that typically are as high as the R peak. And connecting, disconnecting the RL electrode doesn't change anything suggesting that the RLD drive doesn't work.
Is there something I did wrong regardind the electronic design, the registers ?
Thanks in advance,
Grégoire