Other Parts Discussed in Thread: ADS7054, ADS7056
Hello team,
I'm working on a design that utilizes the ADS7851 and Beaglebone Black for data acquisition. I'm a bit unfamiliar with SPI communication so I am a little confused on how to wire up these devices.
The ADS7851 has two SDO SPI outputs: SDO-B, SDO-A
and two SPI inputs: SCLK and CS
The Beaglebone Black has two SPI intefaces on the expansion header:
####SPI0 :
- CS0 : P9_17
- MISO : P9_21
- MOSI : P9_18
- SCLK : P9_22
####SPI1 :
- CS0 : P9_28
- CS1 : P9_42
- MISO : P9_29
- MOSI : P9_30
- SCLK : P9_31
Would it be okay to make these connections from the ADC7851 to the Beaglebone Black expansion header?:
SDO-A to P9_21
SDO-B to P9_29
SCLK to P9_31
CS to P9_28
Regards,
I.K.