Other Parts Discussed in Thread: ADS8861
I posted about this in September and Evan Sawyer kindly responed:
https://e2e.ti.com/support/data_converters/precision_data_converters/f/73/t/625978
I am now in a position to add the additional information requested, but the thread is locked and I can see no way to request that it be unlocked. So, I am continuing here, please feel free to move this to the original thread.
So I have finally got working boards and time to investigate this further. The boards have had the AVDD supply set to 3.3V and have had the ADC ICs replaced with new parts. The problem is still occuring with all three ADCs needing to be run through one conversion before they will release the SDO line The SPI signal lines on power-up look like this:
The 6V is simply the system supply, AVDD and DVDD are the ADC supplies.
With the VREF supply this is:
VREF looks way too slow to me, but I have another reference laid out which works better:
Again this made no difference, SDO is still stubbornly stuck low on power-up
Any help would be much appreciated.