This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12D1620QML-SP: SDO ibis model

Part Number: ADC12D1620QML-SP

Hello,

I'm trying to simulate the SDO signal using hyperlinx.

I'm using the ibis model of the ADC12D1x00.ibs model.

for some reason during signal changes (low to high & high to low) the signal transition is far from being smooth.

see attached file.

I tried different series transistors and only when I tried very large resistors (200ohm) the signal transition became smooth.

it suggests that it is not an issue of impedance matching (the TL impedance is 50ohms), but rather a driver issue.

Does this make sense? is the ibis model correct?

regards,

ItaiAD12D1620_Hyperlinx_Simulation.pdf