ADS21While evaluating the ADS1271 shorted-input noise I encountered very significant 3 to 4 Hz periodic noise. The shorted input noise is about 240 counts peak-to-peak (Standard deviation = 40 ) and the periodic noise appears to be around 130 counts peak-to-peak. Is this 3-4 Hz periodic noise a known behavior of the ADS1271? Are there sampling rates or modes that can reduce it? Thank you