Part Number: ADC12DJ3200EVM
Other Parts Discussed in Thread: TSW14J57EVM,
HI,
I'd like to be able to initiate data capture and save data on command from the ADC12DJ3200EVM (most likely using LabVIEW). Is this possible with the TSW14J56EVM /TSW14J57EVM ? I'd like to avoid using the HSDC Pro software unless I am able to interface to it from my LabVIEW code. If not, what would you recommend to accomplish this?
Also, I saw in another forum post that:
"The ADC12DJ3200EVM+TSW14J56EVM combination has limitations on maximum JESD204B data rate of around 10.8 Gbit/sec. This will limit the maximum ADC clock rate in the 12 bit modes of operation (JMODE0, JMODE2) to 2.7 GHz clock rate."
Is that because of the on board clocks? Could I run at max speed supplying external clocks?
Thanks,
Jeremy