This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1263EVM-PDK: ADCPro connection error

Part Number: ADS1263EVM-PDK
Other Parts Discussed in Thread: ADCPRO, DAC9881EVM-PDK, ADS1263

I have tried to test the EVM board on 2 different computers, running Win 7 x64.

As per user guide, I first installed the ADCPro, and then the ADS1262EVM-SW-installer.

I see the NI-VISA driver correctly on Device Manager, but when I open the ADCPro, I get the message 

Download successful
DSP not ready... Retrying

And then it times out.

I have read this tread: https://e2e.ti.com/support/data_converters/precision_data_converters/f/73/p/484857/1749129#1749129

And I installed the v1.0 stand alone version suggested by Christopher Hall, but to no avail.

I am using the power supply that came with the DAC9881EVM-PDK, and I am using the board as it came - didn't change any jumper. I have tried with 2 different USB cables, and at least 4 different USB ports.

If this information helps, MMB0 is rev. D, and BOM is rev. E. ADS1263 board is Rev. A. Also, I have Labview 2016 installed on both computers (hardly matters at all, but go figure those NI-VISA drivers...)