Part Number: DAC7718
Other Parts Discussed in Thread: DAC7716
Dear Team,
On the datasheet of DAC7718, AIDD is given as 7mA(max) in “ELECTRICAL CHARACTERISTICS: Single-Supply (continued)” section. However, Figure 84 max source current looks like to be around 9mA. Could you please take a look and advise which one is relevant?
There are some more questions as follows:
- What is the max current at Vout=12V condition?
- What is the typical efficiency of the device?
- Max short current is given as +/-8mA on the datasheet. The note(5) states as “(5) When the output current is greater than the specification, the current is clamped at the specified maximum value.” What is the max time that the part can be hold at short condition?
- DAC7716 could also be an option, but load current graph and measurements for Unipolar operation is not given on the datasheet. Is it possible to get this information.
Best Regards,
Caglar