This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC38RF82: Fusefarm Autoload sequence done

Part Number: DAC38RF82


Hi,

  • According to a post I found here here:
    "The fusefarm contains an internal prom that is used to load certain registers after a hard reset is issued after power has been stabilized. This must be done every time the DAC is turned on".
  • In our design, AUTOLOAD_DONE field is not set (=0) and EFC_ERR = 00000 (Vendor ID and Chip Version Register (address = 0x7F)).
  • We are following the sequence in figure 141:
    TXENABLE low. All voltages are ok. TRSTB low. DACCLKSE input is provided (9GHz / 1Vpp sine wave via DC block capacitor). RESETB goes low and high.
    In this sequence we also program the device to 4-wire and setting SEL_EXTCLK_DIFFSE=1 (and repeat these two after each RESETB toggle).
  1. What are we doing wrong that AUTOLOAD_DONE is not set?
    How come it is not set while EFC_ERR = 00000? (no errors from the fuse farm)
  2. When Autoload sequence is not done, will it block me from programming certain registers? Or outputting, for example, a divided DAC CLK to CLKTXP/N?
    I was unable to read successfuly what I programmed into  Divided Output Clock Configuration Register (address = 0x0C) and Clock Input and PLL Configuration Register (address = 0x31).

Thank you

Gil

  • Hi Gil,

    We are looking into your questions, and will be back with you soon.

    Best Regards,

    Dan
  • Hi Dan,

    An update to the issue:

    The clock supplied to the DAC (DIFF or SE) should be properly configured using SEL_EXTCLK_DIFFSE (register CLK_PLL_CFG).

    In addition, writing/reading to a register should consider its related page (Table 47).

    Once setting SEL_EXTCLK_DIFFSE (as part of the "Pull TRSTB pin ....." rectangle (see below)), we got AUTOLOAD_DONE=1.

    I suggest input this remark into figure 141.

    thanks

    Gil