Other Parts Discussed in Thread: REF5050, TIPD216
Hi team,
My customer is designing a schematic for a prototype including DAC8775.
I am supposed to suggest a reference schematic to customer on Jan 9.
Since I attached the schematic that I thought, would you mind
checking it?
In addition,the design spec is as follows.
Vin:15V(Single supply)
Output:0~20mA(4ch)
*Voltage output stage is not used.
External load:450Ω max
HART interface:not used
Back-Boost converter:not used
Sincerely,
Tsuyoshi Tokumoto