Part Number: ADS7953
Hi,
I have an ADS7953 in my design, and I had a failure during EMC testing in the EMI chamber during what appears to be BCI at 1MHz. The chip fails in such that all of the channels work for say 50% of the range (almost like there is an offset). So it seems the reference voltage is being messed up? What is causing this?
Some things to note: the REF5025 is putting out a solid 2.5V, the layout is done as is shown in the data sheet, I have 4 unused channels that have the RC filter network on them, however they are floating.
If I replace the chip post failure, everything is fine, so it does seem that something is getting messed up in the chip.
What can I do to improve the robustness of my design to survive BCI?
Thank you!
Josh