Part Number: ADS1292
Hello,
I am trying to interface with the ADS1292R via SPI, however I believe I have a problem with the voltages required to properly interact with the device.
I am powering it with unipolar supplies with AVDD = DVDD = 3.3V. I also setup the circuit recommended on the datasheet for single supply operation with all the mentioned capacitors. I read on the forum that the voltage on VCAP1 should be 1.2V and on VCAP2 it should be AVDD + 1.8V. In fact, I have 1.2V at VCAP1, however I am measuring around 2.6V at VCAP2, which is not close to what I was expecting.
Could this be the reason why the device is not responding? I used a logic analyzer to see that whenever I pull the START line HIGH there are no changes in the DRDY line which leads me to believe that the device isn't properly working.
Do you have any idea of what I might be doing wrong?
Thank you,
Margarida