This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/TVP5146EVM: TVP5146

Part Number: TVP5146EVM
Other Parts Discussed in Thread: TVP5146

Tool/software: Linux

Hi

I have TVP5146 and leopardboard.I read data TVP5146 and I did the configuration.But ı see entirely green frame.How can ı fix it.

I configured the tvp514x.c file as shown in the picture.

This is how the video frame looks;

  • This looks more like a host processor side configuration issue.

    Make sure your processor video port is configured for YUV422.

    Make sure that your processor display path is also configured correctly. Try forcing date into the display buffer for a known color and make sure it gets displayed correctly (i.e. the cyan cross in the middle of your example. I assume this is rendered to your display buffer after image capture? Is it being displayed in the correct color?

    What is your image source? Can you use a color bar test image from a DVD player? What does that look like?

    What is your wiring connectivity from the TVP digital output to the Leopard board? Is the wiring connectivity and Leopard board configuration correct?

    BR,

    Steve

  • Thanks for reply.

    I use a Pal camera and LI-VI365 module(TVP in this module).And I stream to LAN with gstreamer.I watch stream from VLC.