Part Number: ADS1248
Hi,
I would like to ask you following questions about "8.1 Noise performance". (datasheet p21)
Q1) Input-refferred noise
Will you tell me the meaning of "input-refferred noise", for sure?
My understanding is the value of "Output Noise(input is shorted to GND)/PGA gain".
Is this correct?
Q2) Relation betrween input-reffered noise and PGA gain
Why is the "input-reffered noise" is smaller when PGA gain is bigger?
For example, 1.1uVrms @Gain=1, 5SPS > 0.68uVrms @Gain=2, 5SPS.
Is this due to the relation between "Input signal range"(dynamic range) and PGA gain?
Q3) Table 1, 3, 5 (datasheet p21 - p23)
The values on the table are "measurement value", not specification, correct?
Do you have the data in case Ta = -10℃ and +90℃ ?
Thank you for your support.
Best Regards,