This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC121C021: How to preset the pointer?

Part Number: ADC121C021


HI

The datasheet only mentioned how to do immediate read after pointer set.

But if we did not read the register immediately (we want preset the poiter first) how to preset the pointer then afterword go back to read the ADC121C021?

thanks!

  • Hello,

    This is done by first doing a write command and setting the pointer.  This is shown in the top half of Figure 32.  The read command shown in the bottom half of Figure 32 does not need to be done at this time.  Next when you are ready to read the register make a reading of the preset register as shown in Figure 29 or 31.

    Mike

  • Mike,

    In between the preset pointer set and the reading

    1. what will happen if in between if i insert a stop condition ?

    2. is a re-start condition needed to begin my reading ?

    Thanks!

  • Hello,

    It is ok to do the communication shown in the top half of Figure 32 followed by a stop.  When you are ready to read the register the pointer is already set up from your write so you read the register as shown in Figure 29 or 31.

    Mike