Part Number: DAC8734
We have 4 DAC8734's on the board. It has always worked, but after I reworked the board (that does not directly affect these DACs), all 4 DACs developed large output offsets. DAC0 has 100 to 200 mV of offset, DAC1 ~500mV, DAC2 ~300mV, and DAC3 <100mV. All 4 DAC are similar. The offset is not a straight offset because after trying to externally calibrate out this error, there is still ~180mV of error at 0V. I do not follow the power sequence. The power sequence that we use (because of other circuits on the board) is: -15V, +15V, Vref, +3.3V (for both DVdd and IOVdd). I read in the forum that the registers may not start up correctly if the power sequence is not followed, so I applied reset to the RST input, but the offsets remained. In the forum, I also read that there has been no permanent damaged observed with wrong power sequence. Can you tell me what is happening with my DACs?