Other Parts Discussed in Thread: ADS1298
Hello. I'm working in a project with the ADS1298. I need some help to understand something about the data rate and time settle:
If im trying to have a 500 SPS (24+24*8 bits ready to be taken by spi, every 2ms), so DRDY should toggle to 0 every 2ms...when I see the t settle table
in the datasheet ( p. 51) it shows a time settle (when DRDY should toggle to 0 to indicate new data) of 18440/2048000 = 9ms...that is a data rate of 111 SPS
So thats my confusion...which is the correct data rate (I understand data rate as have the 24+24*8 bits ready)? 500 sps or 111 sps?
Thank you.