This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1298ECGFE-PDK: ADS1298

Part Number: ADS1298ECGFE-PDK

I want to interface ADS1298ECG-PDK with arduino can you please give me the sorce code for this. 

  • Hello Ahmed,

    Thanks for your post. Links to download the firmware and GUI source code for the ADS1298ECGFE-PDK can be found on the EVM product folder. This is the only example code we can provide. Unfortunately, we do not have anything specifically for Arduino.

    Best Regards,
  • I found a arduino code from internet but not sure that weather it works well or not, kindly look at the code and suggest me.

    here are code attach file
    /*
     * adsCMD.h
     * Library header file for adsCMD library
     */
    #include "Arduino.h"
    
    //For Leonardo SPI see http://openenergymonitor.blogspot.com/2012/06/arduino-leonardo-atmega32u4-and-rfm12b.html
    //constants define pins on Arduino 
    
    // Arduino Due
    const int IPIN_PWDN = 47; //not required for TI demo kit
    const int PIN_CLKSEL = 49;//6;//*optional
    const int IPIN_RESET  = 48;//*optional
    
    const int PIN_START = 46;
    const int IPIN_DRDY = 45;
    const int IPIN_CS = 52;
    //const int PIN_DOUT = 11;//SPI out
    //const int PIN_DIN = 12;//SPI in
    //const int PIN_SCLK = 13;//SPI clock
    
    //function prototypes
    void adc_wreg(int reg, int val); //write register
    void adc_send_command(int cmd); //send command
    int adc_rreg(int reg); //read register
    
    
    
    
    
    
    
    /* adsCMD.cpp
     * simple library to light an LED for a duration given in milliseconds
     */
    #include "Arduino.h"   // use: Wprogram.h for Arduino versions prior to 1.0
    #include "adsCMD.h"
    #include "ads1298.h"
    #include <SPI.h>  // include the SPI library:
    
    
    
    void adc_send_command(int cmd)
    {
    	digitalWrite(IPIN_CS, LOW);
    	SPI.transfer(cmd);
    	delayMicroseconds(1);
    	digitalWrite(IPIN_CS, HIGH);
    }
    
    void adc_wreg(int reg, int val)
    {
      //see pages 40,43 of datasheet - 
    	digitalWrite(IPIN_CS, LOW);
    	SPI.transfer(ADS1298::WREG | reg);
    	SPI.transfer(0);	// number of registers to be read/written � 1
    	SPI.transfer(val);
    	delayMicroseconds(1);
    	digitalWrite(IPIN_CS, HIGH);
    }
    
    int adc_rreg(int reg){
      int out = 0;
      digitalWrite(IPIN_CS, LOW);
      SPI.transfer(ADS1298::RREG | reg);
      delayMicroseconds(5);
      SPI.transfer(0);	// number of registers to be read/written � 1
      delayMicroseconds(5);
      out = SPI.transfer(0);
      	delayMicroseconds(1);
    
    
    
    
    
    
    #ifndef ADS1298_H
    #define ADS1298_H
    
    #ifdef __cplusplus
    namespace ADS1298 {
    #endif
    
    	enum spi_command {
    		// system commands
    		WAKEUP = 0x02,
    		STANDBY = 0x04,
    		RESET = 0x06,
    		START = 0x08,
    		STOP = 0x0a,
    
    		// read commands
    		RDATAC = 0x10,
    		SDATAC = 0x11,
    		RDATA = 0x12,
    
    		// register commands
    		RREG = 0x20,
    		WREG = 0x40
    	};
    
    	enum reg {
    		// device settings
    		ID = 0x00,
    
    		// global settings
    		CONFIG1 = 0x01,
    		CONFIG2 = 0x02,
    		CONFIG3 = 0x03,
    		LOFF = 0x04,
    
    		// channel specific settings
    		CHnSET = 0x04,
    		CH1SET = CHnSET + 1,
    		CH2SET = CHnSET + 2,
    		CH3SET = CHnSET + 3,
    		CH4SET = CHnSET + 4,
    		CH5SET = CHnSET + 5,
    		CH6SET = CHnSET + 6,
    		CH7SET = CHnSET + 7,
    		CH8SET = CHnSET + 8,
    		RLD_SENSP = 0x0d,
    		RLD_SENSN = 0x0e,
    		LOFF_SENSP = 0x0f,
    		LOFF_SENSN = 0x10,
    		LOFF_FLIP = 0x11,
    
    		// lead off status
    		LOFF_STATP = 0x12,
    		LOFF_STATN = 0x13,
    
    		// other
    		GPIO = 0x14,
    		PACE = 0x15,
    		RESP = 0x16,
    		CONFIG4 = 0x17,
    		WCT1 = 0x18,
    		WCT2 = 0x19
    	};
    
    	enum ID_bits {
    		DEV_ID7 = 0x80,
    		DEV_ID6 = 0x40,
    		DEV_ID5 = 0x20,
    		DEV_ID2 = 0x04,
    		DEV_ID1 = 0x02,
    		DEV_ID0 = 0x01,
    
    		ID_const = 0x10,
    		ID_ADS129x = DEV_ID7,
    		ID_ADS129xR = (DEV_ID7 | DEV_ID6),
    
    		ID_4CHAN = 0,
    		ID_6CHAN = DEV_ID0,
    		ID_8CHAN = DEV_ID1,
    
    		ID_ADS1294 = (ID_ADS129x | ID_4CHAN),
    		ID_ADS1296 = (ID_ADS129x | ID_6CHAN),
    		ID_ADS1298 = (ID_ADS129x | ID_8CHAN),
    		ID_ADS1294R = (ID_ADS129xR | ID_4CHAN),
    		ID_ADS1296R = (ID_ADS129xR | ID_6CHAN),
    		ID_ADS1298R = (ID_ADS129xR | ID_8CHAN)
    	};
    
    	enum CONFIG1_bits {
    		HR = 0x80,
    		DAISY_EN = 0x40,
    		CLK_EN = 0x20,
    		DR2 = 0x04,
    		DR1 = 0x02,
    		DR0 = 0x01,
    
    		CONFIG1_const = 0x00,
    		HIGH_RES_32k_SPS = HR,
    		HIGH_RES_16k_SPS = (HR | DR0),
    		HIGH_RES_8k_SPS = (HR | DR1),
    		HIGH_RES_4k_SPS = (HR | DR1 | DR0),
    		HIGH_RES_2k_SPS = (HR | DR2),
    		HIGH_RES_1k_SPS = (HR | DR2 | DR0),
    		HIGH_RES_500_SPS = (HR | DR2 | DR1),
    		LOW_POWR_250_SPS = (DR2 | DR1)
    	};
    
    	enum CONFIG2_bits {
    		WCT_CHOP = 0x20,
    		INT_TEST = 0x10,
    		TEST_AMP = 0x04,
    		TEST_FREQ1 = 0x02,
    		TEST_FREQ0 = 0x01,
    
    		CONFIG2_const = 0x00,
    		INT_TEST_4HZ = INT_TEST, 
    		INT_TEST_8HZ = (INT_TEST | TEST_FREQ0),
    		INT_TEST_DC = (INT_TEST | TEST_FREQ1 | TEST_FREQ0)
    	};
    
    	enum CONFIG3_bits {
    		PD_REFBUF = 0x80,
    		VREF_4V = 0x20,
    		RLD_MEAS = 0x10,
    		RLDREF_INT = 0x08,
    		PD_RLD = 0x04,
    		RLD_LOFF_SENS = 0x02,
    		RLD_STAT = 0x01,
    
    		CONFIG3_const = 0x40
    	};
    
    	enum LOFF_bits {
    		COMP_TH2 = 0x80,
    		COMP_TH1 = 0x40,
    		COMP_TH0 = 0x20,
    		VLEAD_OFF_EN = 0x10,
    		ILEAD_OFF1 = 0x08,
    		ILEAD_OFF0 = 0x04,
    		FLEAD_OFF1 = 0x02,
    		FLEAD_OFF0 = 0x01,
    
    		LOFF_const = 0x00,
    
    		COMP_TH_95 = 0x00,
    		COMP_TH_92_5 = COMP_TH0,
    		COMP_TH_90 = COMP_TH1,
    		COMP_TH_87_5 = (COMP_TH1 | COMP_TH0),
    		COMP_TH_85 = COMP_TH2,
    		COMP_TH_80 = (COMP_TH2 | COMP_TH0),
    		COMP_TH_75 = (COMP_TH2 | COMP_TH1),
    		COMP_TH_70 = (COMP_TH2 | COMP_TH1 | COMP_TH0),
    
    		ILEAD_OFF_6nA = 0x00,
    		ILEAD_OFF_12nA = ILEAD_OFF0,
    		ILEAD_OFF_18nA = ILEAD_OFF1,
    		ILEAD_OFF_24nA = (ILEAD_OFF1 | ILEAD_OFF0),
    
    		FLEAD_OFF_AC = FLEAD_OFF0,
    		FLEAD_OFF_DC = (FLEAD_OFF1 | FLEAD_OFF0)
    	};
    
    	enum CHnSET_bits {
    		PDn = 0x80,
    		PD_n = 0x80,
    		GAINn2 = 0x40,
    		GAINn1 = 0x20,
    		GAINn0 = 0x10,
    		MUXn2 = 0x04,
    		MUXn1 = 0x02,
    		MUXn0 = 0x01,
    
    		CHnSET_const = 0x00,
    
    		GAIN_1X = GAINn0,
    		GAIN_2X = GAINn1,
    		GAIN_3X = (GAINn1 | GAINn0),
    		GAIN_4X = GAINn2,
    		GAIN_6X = 0x00,
    		GAIN_8X = (GAINn2 | GAINn0),
    		GAIN_12X = (GAINn2 | GAINn1),
    
    		ELECTRODE_INPUT = 0x00,
    		SHORTED = MUXn0,
    		RLD_INPUT = MUXn1,
    		MVDD = (MUXn1 | MUXn0),
    		TEMP = MUXn2,
    		TEST_SIGNAL = (MUXn2 | MUXn0),
    		RLD_DRP = (MUXn2 | MUXn1),
    		RLD_DRN = (MUXn2 | MUXn1 | MUXn0)
    	};
    
    	enum CH1SET_bits {
    		PD_1 = 0x80,
    		GAIN12 = 0x40,
    		GAIN11 = 0x20,
    		GAIN10 = 0x10,
    		MUX12 = 0x04,
    		MUX11 = 0x02,
    		MUX10 = 0x01,
    
    		CH1SET_const = 0x00
    	};
    
    	enum CH2SET_bits {
    		PD_2 = 0x80,
    		GAIN22 = 0x40,
    		GAIN21 = 0x20,
    		GAIN20 = 0x10,
    		MUX22 = 0x04,
    		MUX21 = 0x02,
    		MUX20 = 0x01,
    
    		CH2SET_const = 0x00
    	};
    
    	enum CH3SET_bits {
    		PD_3 = 0x80,
    		GAIN32 = 0x40,
    		GAIN31 = 0x20,
    		GAIN30 = 0x10,
    		MUX32 = 0x04,
    		MUX31 = 0x02,
    		MUX30 = 0x01,
    
    		CH3SET_const = 0x00
    	};
    
    	enum CH4SET_bits {
    		PD_4 = 0x80,
    		GAIN42 = 0x40,
    		GAIN41 = 0x20,
    		GAIN40 = 0x10,
    		MUX42 = 0x04,
    		MUX41 = 0x02,
    		MUX40 = 0x01,
    
    		CH4SET_const = 0x00
    	};
    
    	enum CH5SET_bits {
    		PD_5 = 0x80,
    		GAIN52 = 0x40,
    		GAIN51 = 0x20,
    		GAIN50 = 0x10,
    		MUX52 = 0x04,
    		MUX51 = 0x02,
    		MUX50 = 0x01,
    
    		CH5SET_const = 0x00
    	};
    
    	enum CH6SET_bits {
    		PD_6 = 0x80,
    		GAIN62 = 0x40,
    		GAIN61 = 0x20,
    		GAIN60 = 0x10,
    		MUX62 = 0x04,
    		MUX61 = 0x02,
    		MUX60 = 0x01,
    
    		CH6SET_const = 0x00
    	};
    
    	enum CH7SET_bits {
    		PD_7 = 0x80,
    		GAIN72 = 0x40,
    		GAIN71 = 0x20,
    		GAIN70 = 0x10,
    		MUX72 = 0x04,
    		MUX71 = 0x02,
    		MUX70 = 0x01,
    
    		CH7SET_const = 0x00
    	};
    
    	enum CH8SET_bits {
    		PD_8 = 0x80,
    		GAIN82 = 0x40,
    		GAIN81 = 0x20,
    		GAIN80 = 0x10,
    		MUX82 = 0x04,
    		MUX81 = 0x02,
    		MUX80 = 0x01,
    
    		CH8SET_const = 0x00
    	};
    
    	enum RLD_SENSP_bits {
    		RLD8P = 0x80,
    		RLD7P = 0x40,
    		RLD6P = 0x20,
    		RLD5P = 0x10,
    		RLD4P = 0x08,
    		RLD3P = 0x04,
    		RLD2P = 0x02,
    		RLD1P = 0x01,
    
    		RLD_SENSP_const = 0x00
    	};
    
    	enum RLD_SENSN_bits {
    		RLD8N = 0x80,
    		RLD7N = 0x40,
    		RLD6N = 0x20,
    		RLD5N = 0x10,
    		RLD4N = 0x08,
    		RLD3N = 0x04,
    		RLD2N = 0x02,
    		RLD1N = 0x01,
    
    		RLD_SENSN_const = 0x00
    	};
    
    	enum LOFF_SENSP_bits {
    		LOFF8P = 0x80,
    		LOFF7P = 0x40,
    		LOFF6P = 0x20,
    		LOFF5P = 0x10,
    		LOFF4P = 0x08,
    		LOFF3P = 0x04,
    		LOFF2P = 0x02,
    		LOFF1P = 0x01,
    
    		LOFF_SENSP_const = 0x00
    	};
    
    	enum LOFF_SENSN_bits {
    		LOFF8N = 0x80,
    		LOFF7N = 0x40,
    		LOFF6N = 0x20,
    		LOFF5N = 0x10,
    		LOFF4N = 0x08,
    		LOFF3N = 0x04,
    		LOFF2N = 0x02,
    		LOFF1N = 0x01,
    
    		LOFF_SENSN_const = 0x00
    	};
    
    	enum LOFF_FLIP_bits {
    		LOFF_FLIP8 = 0x80,
    		LOFF_FLIP7 = 0x40,
    		LOFF_FLIP6 = 0x20,
    		LOFF_FLIP5 = 0x10,
    		LOFF_FLIP4 = 0x08,
    		LOFF_FLIP3 = 0x04,
    		LOFF_FLIP2 = 0x02,
    		LOFF_FLIP1 = 0x01,
    
    		LOFF_FLIP_const = 0x00
    	};
    
    	enum LOFF_STATP_bits {
    		IN8P_OFF = 0x80,
    		IN7P_OFF = 0x40,
    		IN6P_OFF = 0x20,
    		IN5P_OFF = 0x10,
    		IN4P_OFF = 0x08,
    		IN3P_OFF = 0x04,
    		IN2P_OFF = 0x02,
    		IN1P_OFF = 0x01,
    
    		LOFF_STATP_const = 0x00
    	};
    
    	enum LOFF_STATN_bits {
    		IN8N_OFF = 0x80,
    		IN7N_OFF = 0x40,
    		IN6N_OFF = 0x20,
    		IN5N_OFF = 0x10,
    		IN4N_OFF = 0x08,
    		IN3N_OFF = 0x04,
    		IN2N_OFF = 0x02,
    		IN1N_OFF = 0x01,
    
    		LOFF_STATN_const = 0x00
    	};
    
    	enum GPIO_bits {
    		GPIOD4 = 0x80,
    		GPIOD3 = 0x40,
    		GPIOD2 = 0x20,
    		GPIOD1 = 0x10,
    		GPIOC4 = 0x08,
    		GPIOC3 = 0x04,
    		GPIOC2 = 0x02,
    		GPIOC1 = 0x01,
    
    		GPIO_const = 0x00
    	};
    
    	enum PACE_bits {
    		PACEE1 = 0x10,
    		PACEE0 = 0x08,
    		PACEO1 = 0x04,
    		PACEO0 = 0x02,
    		PD_PACE = 0x01,
    
    		PACE_const = 0x00,
    
    		PACEE_CHAN2 = 0x00,
    		PACEE_CHAN4 = PACEE0,
    		PACEE_CHAN6 = PACEE1,
    		PACEE_CHAN8 = (PACEE1 | PACEE0),
    
    		PACEO_CHAN1 = 0x00,
    		PACEO_CHAN3 = PACEE0,
    		PACEO_CHAN5 = PACEE1,
    		PACEO_CHAN7 = (PACEE1 | PACEE0)
    	};
    
    	enum RESP_bits {
    		RESP_DEMOD_EN1 = 0x80,
    		RESP_MOD_EN1 = 0x40,
    		RESP_PH2 = 0x10,
    		RESP_PH1 = 0x08,
    		RESP_PH0 = 0x04,
    		RESP_CTRL1 = 0x02,
    		RESP_CTRL0 = 0x01,
    
    		RESP_const = 0x20,
    
    		RESP_PH_22_5 = 0x00,
    		RESP_PH_45 = RESP_PH0,
    		RESP_PH_67_5 = RESP_PH1,
    		RESP_PH_90 = (RESP_PH1 | RESP_PH0),
    		RESP_PH_112_5 = RESP_PH2,
    		RESP_PH_135 = (RESP_PH2 | RESP_PH0),
    		RESP_PH_157_5 = (RESP_PH2 | RESP_PH1),
    
    		RESP_NONE = 0x00,
    		RESP_EXT = RESP_CTRL0,
    		RESP_INT_SIG_INT = RESP_CTRL1,
    		RESP_INT_SIG_EXT = (RESP_CTRL1 | RESP_CTRL0)
    	};
    
    	enum CONFIG4_bits {
    		RESP_FREQ2 = 0x80,
    		RESP_FREQ1 = 0x40,
    		RESP_FREQ0 = 0x20,
    		SINGLE_SHOT = 0x08,
    		WCT_TO_RLD = 0x04,
    		PD_LOFF_COMP = 0x02,
    
    		CONFIG4_const = 0x00,
    
    		RESP_FREQ_64k_Hz = 0x00,
    		RESP_FREQ_32k_Hz = RESP_FREQ0,
    		RESP_FREQ_16k_Hz = RESP_FREQ1,
    		RESP_FREQ_8k_Hz = (RESP_FREQ1 | RESP_FREQ0),
    		RESP_FREQ_4k_Hz = RESP_FREQ2,
    		RESP_FREQ_2k_Hz = (RESP_FREQ2 | RESP_FREQ0),
    		RESP_FREQ_1k_Hz = (RESP_FREQ2 | RESP_FREQ1),
    		RESP_FREQ_500_Hz = (RESP_FREQ2 | RESP_FREQ1 | RESP_FREQ0)
    	};
    
    	enum WCT1_bits {
    		aVF_CH6 = 0x80,
    		aVL_CH5 = 0x40,
    		aVR_CH7 = 0x20,
    		avR_CH4 = 0x10,
    		PD_WCTA = 0x08,
    		WCTA2 = 0x04,
    		WCTA1 = 0x02,
    		WCTA0 = 0x01,
    
    		WCT1_const = 0x00,
    
    		WCTA_CH1P = 0x00,
    		WCTA_CH1N = WCTA0,
    		WCTA_CH2P = WCTA1,
    		WCTA_CH2N = (WCTA1 | WCTA0),
    		WCTA_CH3P = WCTA2,
    		WCTA_CH3N = (WCTA2 | WCTA0),
    		WCTA_CH4P = (WCTA2 | WCTA1),
    		WCTA_CH4N = (WCTA2 | WCTA1 | WCTA0)
    	};
    
    	enum WCT2_bits {
    		PD_WCTC = 0x80,
    		PD_WCTB = 0x40,
    		WCTB2 = 0x20,
    		WCTB1 = 0x10,
    		WCTB0 = 0x08,
    		WCTC2 = 0x04,
    		WCTC1 = 0x02,
    		WCTC0 = 0x01,
    
    		WCT2_const = 0x00,
    
    		WCTB_CH1P = 0x00,
    		WCTB_CH1N = WCTB0,
    		WCTB_CH2P = WCTB1,
    		WCTB_CH2N = (WCTB1 | WCTB0),
    		WCTB_CH3P = WCTB2,
    		WCTB_CH3N = (WCTB2 | WCTB0),
    		WCTB_CH4P = (WCTB2 | WCTB1),
    		WCTB_CH4N = (WCTB2 | WCTB1 | WCTB0),
    
    		WCTC_CH1P = 0x00,
    		WCTC_CH1N = WCTC0,
    		WCTC_CH2P = WCTC1,
    		WCTC_CH2N = (WCTC1 | WCTC0),
    		WCTC_CH3P = WCTC2,
    		WCTC_CH3N = (WCTC2 | WCTC0),
    		WCTC_CH4P = (WCTC2 | WCTC1),
    		WCTC_CH4N = (WCTC2 | WCTC1 | WCTC0)
    	};
    
    #ifdef __cplusplus
    }
    #endif /* namespace ADS1298 */
    
    #endif				/* ADS1298_H */
    
    
    
    
    
    
    
    // Minimal sketch for connection to ADS129n family. Load this script and open Tools/SerialMonitor. 
    // You should see text like this
    //  Device Type (ID Control Register): 62 Channels: 8
    // If you see "Channels: 0" then check your wiring
    
    #include "ads1298.h"
    #include "adsCMD.h"
    #include <SPI.h>  // include the SPI library:
    int gMaxChan = 0; //maximum number of channels supported by ads129n = 4,6,8
    int gIDval = 0; //Device ID : lower 5 bits of  ID Control Register 
    
    int activeSerialPort = 0; //data will be sent to serial port that last sent commands. E.G. bluetooth or USB port
    const int kPIN_LED = 13;//pin with in-built light - typically 13, 11 for Teensy 2.0. 
    
    #if defined(__SAM3X8E__)
      #define isDUE  //Detect Arduino Due
      //#define WiredSerial SerialUSB //Use Due's Native port
      #define WiredSerial Serial
    #else  
      #define WiredSerial Serial
    #endif
    
    void setup(){
      using namespace ADS1298;
      //prepare pins to be outputs or inputs
      //pinMode(PIN_SCLK, OUTPUT); //optional - SPI library will do this for us
      //pinMode(PIN_DIN, OUTPUT); //optional - SPI library will do this for us
      //pinMode(PIN_DOUT, INPUT); //optional - SPI library will do this for us
      pinMode(IPIN_CS, OUTPUT);
      pinMode(PIN_START, OUTPUT);
      pinMode(IPIN_DRDY, INPUT);
      pinMode(PIN_CLKSEL, OUTPUT);//*optional
      pinMode(IPIN_RESET, OUTPUT);//*optional
      pinMode(IPIN_PWDN, OUTPUT);//*optional
      //start Serial Peripheral Interface
      SPI.begin();
      SPI.setBitOrder(MSBFIRST);
      #ifndef isDUE
      SPI.setClockDivider(SPI_CLOCK_DIV4); //http://forum.pjrc.com/threads/1156-Teensy-3-SPI-Basic-Clock-Questions
      #endif
      SPI.setDataMode(SPI_MODE1);
      //Start ADS1298
      delay(500); //wait for the ads129n to be ready - it can take a while to charge caps
      adc_send_command(SDATAC); // Send SDATAC Command (Stop Read Data Continuously mode)
      delay(10);
      // Determine model number and number of channels available
      gIDval = adc_rreg(ID); //lower 5 bits of register 0 reveal chip type
      switch (gIDval & B00011111 ) { //least significant bits reports channels
              case  B10000: //16
                gMaxChan = 4; //ads1294
                break;
              case B10001: //17
                gMaxChan = 6; //ads1296
                break; 
              case B10010: //18
                gMaxChan = 8; //ads1298
                break;
              case B11110: //30
                gMaxChan = 8; //ads1299
                break;
              default: 
                gMaxChan = 0;
      }
      //start serial port
      WiredSerial.begin(115200); //use native port on Due
      while (WiredSerial.read() >= 0) {} //http://forum.arduino.cc/index.php?topic=134847.0
      //while (!WiredSerial) ; //required by Leonardo http://arduino.cc/en/Serial/IfSerial (ads129n requires 3.3v signals, Leonardo is 5v)
      delay(200);  // Catch Due reset problem
      pinMode(kPIN_LED, OUTPUT); 
    }
    
    void loop()
    {
      WiredSerial.print("Device Type (ID Control Register): "); WiredSerial.print(gIDval); WiredSerial.print(" Channels: "); WiredSerial.println(gMaxChan);
      digitalWrite(kPIN_LED, HIGH);   // turn the LED on (HIGH is the voltage level)
      if (gMaxChan > 0)
        delay(500); //long pause if OK
      else
        delay(50); //rapid blink if error
      digitalWrite(kPIN_LED, LOW);    // turn the LED off by making the voltage LOW
      delay(500); 
    }
    
    
    
    
    
    
    
      digitalWrite(IPIN_CS, HIGH);
      return(out);
    }