Hi,
I would like to have some precisions with the PGA411 circuit .
Could we connect a external exciter on the ie1 ans ie2 inputs without using the internal amplifier?
The idea is to using a brushless motor drive controller to product the excitation signal.
What are the PGA411 registers configuration to have?
: Internal PGA exciter switch off, avoid fault detection.. etc.
Regards,
Pascal