Part Number: ADS1299EEGFE-PDK
Other Parts Discussed in Thread: ADS1299
Hello.
I got a 2Hz, 20μV sine signal connected to the 1299EVM's REF and CH1 + (sample rate at 250Hz). However, when the human body passes by the acquisition device, there is a great disturbance in the collected signals. The waveforms in the figure below are the result after baseline removing and a 50Hz notch filter. Figure 1 is the normal acquisition of the sine wave, Figure 2 shows the waveform of channel 1 when someone walked by. Each irregular peak was caused by walking by. Figure 3 shows the waveform of another Input-shorted channel, which can be seen to be very disturbing.
I've done a lot of experiments with the devices and found that singal gets abnormal when the human body walks past the device, or someone is shaking a leg, or someone is jumping nearby,or even just someone is swing nearby. Moreover, there is still such a problem when using an aluminum box to swing around the acquisition circuit.
Based on the above questions, I’m confused with the EVM. Would you like to show me some solutions for such kind of problems?
Thank you.