This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RE: ADS1013 with AM335x

Other Parts Discussed in Thread: ADS1013, ADS1015

Hi,
I am using ads1013 using in am335x. Is the same source i am using from ads1015 to ads1013. the same ads1015 i can use the same software logic.
is there any settings for this..
regards
  • Lofna,


    I've split off your post from the original thread and started a new thread.

    The ADS1013 is a variant of the ADS1015 without the multiplexer, PGA and comparator. Running the ADS1013 would be the same as running the ADS1015 without using those features, so the same code could be used. Writing to bits that control these features (14:12, 11:9, and 4:0 in the configuration register) would not change operation in the device. You should be able to use the same source code to control the ADS1013.


    Joseph Wu