This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1115: Question of ADS1115's I2C Input Capacitance

Part Number: ADS1115

Hi Sirs,

Would you please advise the input capacitance specification of the ADS1115's I2C pins (SDA, SCL)?

Thank you and Best regards,

Wayne Chen
01/24/2018

  • Wayne,


    The pin capacitance for the ADS1115 I2C pins is modeled in the ADS1115 IBIS model. You can find the model here:

    www.ti.com/.../sbam025

    For information about the IBIS model structure, you can find information in this document:

    www.ti.com/.../snla046.pdf

    For a simple answer, the capacitance for the SDA and SCL lines are approximately 1.5 to 2pF each. There is some difference between the DGS and RUG packages, but the value is similar. I would note that the PCB trace lines often have more capacitance than the device themselves


    Joseph Wu