Part Number: DAC38J84EVM
Other Parts Discussed in Thread: LMK04828, DAC38J84
Hello,
I am trying to program DAC38J8$ EVM using spi connections on the FMC connector.
Firstly, I want to understand signal routing.
I am doing all experiments with GUI software and probing signals.
Is LMK04828 being used as three pin spi interface or a four pin.
According to CPLD RTL code, you seem to using it in 4 pin mode with sdo being connected to read data.
Is that correct?
But, I do not see any data on pin 6 of LMK SPI header J25.It is always high.
Can you tell me how the read signal is getting routed?
Thanks and Regards,
Mallesh