Other Parts Discussed in Thread: TLC3541, OMAP3530
Hello everybody!
I have a problem which I can solve with my software. However, I would like to know the reason this happens.
I have been using a TLC3541 and my signal is just an exponential decay, the period of my signal is 77ms (13Hz) and the clock for my ADC through the SPI interface gives me a 133KSPS which is less than the maximum 200KSPS for the ADC.
When I plot the digitalized signal, it looks exactly how it should be, except that there are some random points reaching the ADC full scale (5V). What is happening there?
Thanks a lot!
The following graph shows this problem: