This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1241: ads1241

Part Number: ADS1241


hi all   

    The product used two ads1421 for pressure transmitter, two ads1241 together sample.but these IC output date are difference.if move first sampling transfer data,it's ok.

  • Davy,


    I'm sorry, but I'm not sure I understand the question. It looks like there are you are using two ADS1241s and you get different data from each reading the same thing?

    I suspect this is some sort of communication problem. However, to help debug your problem I'll need more information about everything in the system. I need a detailed description of the problem in the readout. If the data is bad, then I would need to know the expected result and bad result. If there are cases where the data is good for both devices, I need to know if there are any differences in the read method.

    Also I would need to know the timing of how each device starts a command and the timing for the readout. Scope shots or an output of a logic analyzer would be very helpful in debugging this type of problem. A schematic for the circuit might also give more detail to the solution.

    Regardless, start with a detailed description of the problem, and we can try to debug it.


    Joseph Wu
  • Davy,


    I haven't gotten a reply from you about your data problem. I've given a couple of things to consider, and I hope you've gotten the correct data out. I'll close out this post for now, but if you are still having problems, feel free to post back to reopen the thread.


    Joseph Wu