Part Number: ADS1262
Other Parts Discussed in Thread: TIDA-00550,
Hello, I have an universal external sensor input module that I'm designing with an AFE based on the reference TIDA-00550. I have a custom board and software working, but am getting accuracy results over temperature much worse than the reference design.
I have done gain compensation at room temperature only, and am getting errors around 0.05%FSR at room (which is acceptable for the application). Over temperature the error goes up to 0.9%FSR at 85C (while the reference design stays within 0.05% throughout).
The graph is representative of the results I am getting. It is current measurement from -20mA to +20mA, with a PGA of 4. The accuracy results are pretty much the same regardless of whether I am measuring voltage or current. They are also the same regardless of the PGA value.
I am looking for any ideas or further testing to do in order to narrow down the cause of the additional errors.
Thanks,
Caleb