Part Number: ADC32RF45
Hello,
I have 2 questions regarding register writes and reads for ADC32RF45. I made sure that ADC32RF45 receives both the sampling clock and sysref.
1) Should I put a delay in between register writes or in between page switches or anything of that sort.
2) I write registers x"4002" x"00", x"4003" x"00", x"4004" x"68" to select Main digital page A. However when I read back these registers all I get is x"00". I enter the address as x"4004" to read register back. What am I doing wrong?