Part Number: ADS42JB69
Other Parts Discussed in Thread: DS90LV001, LMK04828,
Quick question regarding the SYNC & SYSREF inputs to the ADS42JB69.
The DS90LV001 LVDS buffer will be used to drive these signals from an FPGA, but we want to confirm the compatibility of the interface. Here are the DS90’s LVDS driver specs:
Even though the AD42JB69 only gives a typical LVDS levels (Hi =1.3V, Lo = 0.5V, Vcm = 0.9V), I assume it can receive the DS90LV001 buffer's LVDS differential signal range. Is this correct?
The common mode voltages do not align: 1.19V for the DS90 and 0.9V for the ADS. I assume this means the signals must be AC coupled. Please confirm.