We have a test setup with the ADC08D1520 located on the main board and the ADC input clock source (CLK+/-) on a daughter board. In our testing we have found that when this ADC input clock source is removed, we can still successfully read the test pattern and our FPGA can lock on the ADC output clock. This seems to imply that the ADC is generating its own output clock.
Can the ADC08D1520 generate its own output clock? We could not find any mention of this capability in the data sheet. If it can generate its own output clock, what determines when it is on or off?
If it can't generate its own clock, should we expect to see a test pattern if the input clock pins are left floating?
Thanks.