Part Number: THS10064
Other Parts Discussed in Thread: TLV571
If there roadmap for ADC matching below specification, please let me know.
--------------------------------------
・5Vcc and near 5V input range
・8bit
・Interface: Parallel output
・Internal reference
・Sample rate: 1Msps
・Package: small as possible and read type
--------------------------------------
I didn't find match IC and competitor have not, too. (Near device is Maxim: MAX154, but external reference)
Second question, if there no matched roadmap IC's, I will promote THS10064(10bit) and explain unused D8 and D9 pin, is this idea correct?
If correct, should unused D8 and D9 connect GND?
Best regards,
Satoshi