Hi Jim Seton and/ or Eben Dwobeng:
I'm having a problem very similar to that reported by Ivan Komsic on 25 April 2017. I'm following the example contained in the DAC38RF8x User's Guide (slau671a.pdf), except that I'm trying to used the on-board VCXO (running at 122.88 MHz).
I'm running:
>Windows 10 (region settings = United States, Language=English)
>Labview RTE 2014 SP1
>RF38RF82EVM GUI
>HSDC Pro Gui (w/ a TSW14J56EVM board)
>2 separate power supplies (each capable of putting out 3 Amps or more)
>all the app notes associated with the TI Hardware and software GUIs mentioned above.
Here's what I *CAN* do:
>Set up the DAC38RF82EVM using the instructions in the User's Guide and the DAC GUI interface
>Output a constant sinusoid tone using the Constant Input mode (3FFF) and the NCO Oscillator
....HOWEVER: the frequency of the tone seems a bit off (using a Signal Hound spectrum analyzer) AND when I ONLY use the Mixer (without NCO) I get a series of tones separated by ~ 400 MHz (just as Ivan Komsic described)
The DAC clock is set to 6144 MHz, just like in the User's Guide example. In using the 122.88 MHz VCXO, I have enabled the PLL (on the overview screen of the DAC38RF82 GUI) and set M=25, N=2 (giving the 6144 MHz DAC clock rate used in DAC38RF8x User's Guide). With some effort, I can tune the PLL to get a PLL LF voltage of 3 or 4, by manually changing the M and N divider values on the "Clocking" tab of the DAC38RF8xEVM GUI.
It seems like I am able to pass information from the TSW14J56EVM board to the DAC38RF82EVM board (no persistent bus errors when I hit "Send" in the HSDC Pro GUI), but I am not able to get the Tx CLK LED to flash (indicator D2, on the TSW14J56EVM board).
If someone could provide some instructions from how to move from the (successful) Constant Input/ NCO tone generation to the (unsuccessful) mixing of a pattern generated by the HSDC Pro GUI/ TSW14J56EVM, I would be extremely grateful. We are trying to evaluate both the DAC38RF82 and a high speed ADC board (maybe the ADC2DJ3200) for a future product, but the difficulties we've encountered so far have made this process very time consuming. Any help you could provide is greatly appreciated.
Thanks,
Steve Krupa