Other Parts Discussed in Thread: ADCPRO, ADS1282
Hi All,
I am working on ADS1282 which is connected to MSP430F2273 over UCA0. I have ADS1282EVM-PDK and use EVM to mount it on standalone system and then use it along with PDK to verify the results on PC. Recently my PDK and EVM have started behaving strange :D. PDK will not work on my laptop but it works on another PC. I have checked all drivers and reinstalled ADCpro with no luck. However, this is not a big problem. Another thing is, EVM when mounted on test board, does not talk to MSP430 at all. I am monitoring all SPI signals and everything looks ok but there is no activity on MISO pin. I am providing 3.2V supply and +-10V supply as well.
I tried reading ID register (address 0x00), then configured different registers and tried to read them, which did not work. I assume ADS1282 is RIP but then why would it work on PDK?
Do you have to change the jumper settings on EVM before you can use it in standalone system? I went through ADS1282EVM-PDK document and it said only thing to change would be J3 if you have external clock source. But here, I am using onboard clock.
I appreciate your time and consideration.
Have a great day !