Hello, I'm using a TVP5150AM1 to decode a composite NTSC video signal that is being transmitted/received over an FM RF link. Occasionally, I see the Lost Lock Detect bit in Status Register #1 go high, along with a mixture of losing the color subcarrier, vertical sync, or horizontal sync lock (one or more of their status bits go low).
Things work perfectly fine if a direct-wired camera is used instead of the FM RF link. I realize this may indicate the real problem lies in the RF link, but I'm looking for any possible ideas that I can try in getting the TVP5150AM1 to deal with the video from the RF link, since it's required in the application.
I've tried forcing both TV and VCR modes, without change. I've also tried forcing NTSC-M mode, again without change.
I've also tried an anti-aliasing filter *close* to what's described in the app note, with 100pF caps and a 10uH inductor (the app note suggests 180pF caps and a 2.7uH inductor). These were the closest values I had nearby--I'm ordering the exact parts but don't have them yet.
Can anyone suggest any other settings to look at and/or modify to see if the decoder can make better use of the "noisy" video?
(I should add that this testing is happening well within the range of the RF link; in other words, I'm not experiencing the lock problems due to the RF link being out of range.)