Hello, I intend to use the ads1247 in a project with 3-wire RTD to measure temperature from 0 to 500 ° C.
I want to use as reference voltage, the Rbias between pins and REFP Refn, the issue of noise.
Some questions:
1
- I have questions regarding the Rcomp in that case I should use a
100ohm resistor (resistance of PT100 at 0 ° C) to adjust my range
between 0 and 500 ° C?
2 - And if due to resistor tolerance, the resistor value is 99ohm (for example), this difference will cause an error, how to fix this?
3
- Setting the current to 1mA of IDAC, the voltage generated by PT100 in
the range of 000-500 ° C is 0-281mV, with a 1.2 Kohm Rbias, the
reference value is 2.4 V (1.2 kohm x ( mA 1mA +1))?
4
- In this case, with PGA equal to 8x, the range will be + -2400mV, but
only used the positive full scale, so are 23-bit resolution for a full
scale of 300mV (~ 558 ° C ), resulting in a resolution of 0.036uV or 0.000067? ok?
Thanks in advance.