Part Number: ADS1230
Hi everyone,
I'm not sure to well understand what does the offset calibration on the ADS1230.
I see two solutions:
1) the ADS1230 creates an internal short to have an input voltage of 0mv and take a measurement. The result should be 0 so if it's not it saves the value as an offset
2) the offset calibration is used to setup a new 0. Let's say the gain is +-19.5mv at 9.75mv I have an output value of 262144. If I run an offset calibration the adc will define and the new value for an input voltage of 9.75mV will be 0?
I'm pretty sur the answer is the first solution, but I would like to be sure.
My application can run during long period and the temperature is not constant. Is it a good solution to periodically run an offset calibration? The offset calibration is it enough to compensate the temperature drift?
Thnk you in advance