This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC8871: Odd behavior, as the DAC is approaching the limits of range it appears to be slipping bits.

Part Number: DAC8871


This is at the full range of the DAC

I am using the DAC8871 with a full range of +/-10 volts on the output.  The following slides show the 10 volt output from the DAC, the 5 volt output from the DAC and the 0 volt output from the DAC.    The same occurs in the negative direction of the output.

 

Power point for TI.pptx