Part Number: ADS8528
Dear Technical Support Team,
Unexpected data appears on DB[15:0] during AVDD =0V.
Normally DB[15:0] are 3.3V when AVDD=5V but about these are about 1.6V when AVDD=0V.
Supply voltages while power-on are following.
AVDD:0V
DVDD:3.3V
HVDD:15V
HVSS:-15V
"Power Supply Recommendations" describes below. Does it affect DB[15:0] ?
----------------------
However, when HVDD is supplied before AVDD, the internal electrostatic discharge (ESD) structure conducts, increasing the IHVDD beyond the specified value until AVDD is applied.
----------------------
Best Regards,
ttd