Part Number: ADS54J66
In the datasheet figure 51 shows a diagram for a recommended input circuit which has 10 ohm resistors connected to the input pins and after the resistor networks but the application diagram figure 144 and the EVM schematic show 5 ohm resistors between the resistor networks.
Which is the preferred connection or does it matter?