Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS5400EVM: to ADC FMC Adapter to Xilinx ZC706 board question

Part Number: ADS5400EVM

Greetings

I am having trouble routing the CLKOUT signal from the ADC board to the ZC706 board and using it as a clock.

The pins I am interested are shown here on the evm,

  

Then routed to the FMC ADC adapter board

Which routes to a non-clock pin on the ZC706

V23   IO_L24P_T3_13            3                  13    NA            NA                  HR        NA
W24   IO_L24N_T3_13            3                  13    NA            NA                  HR        NA

However the DA5(on the EVM) does route to a clock capable pin,

Is my understanding of all this correct?

I my intention was to drive my FPGA with the the output clock from the ADS board.

Thank you!

-Emil C