Part Number: PGA411-Q1
The main problem now is:
1, we need to calculate the cycle time of each FOC in the motor control (interruption cycle 125us). We need to quickly visit whether the state data of the spinning state is available. The fault state that the direct IO can access is only SFAULT total failure, and we can not know the specific state of deterioration and loss of the signal.
2, the LOT and DOS signals compared to AD2S1200 can be accessed quickly by IO, and we hope to have similar access methods on PGA411.