Part Number: ADS1220EVM
Other Parts Discussed in Thread: ADCPRO, , ADS1220
Hello,
I have written a labview GUI to control the EVM because the ADCPro doesnt work at all. My results show there is a drift (downward) after starting to grab real-time data. I have attempted to calibrate out the offset using the MUX setting 14, but this reading actually comes out fine.
Here are my results:
- Actual voltage using Agilent DMM: 0.489V
- Gain: 1
- Samplerate: 20 Hz
- MUX: A0-A1, and for calibration I use Mux (AVdd - AVss)/2
- Referencs: 2.048V
- I take 25 measurements and the take the avg, and subtract it off. The offset comes out to be 16 as an avg, seems logical.
Here is a screen shot of the drift. As soon as a press Run, I do get the exact value but then after a few samples, the reading start to drift, does anyone know what this drift is?