Part Number: ADS54J66
Other Parts Discussed in Thread: ADS54J64
I am asking for confirmation of the JESD Mode and JESD PLL mode of 40x that is given for the LMF = 484 (Mode 0) in Table 13 of the ADS54J66 datasheet.
This is what I can interpret from the ADS54J66 datasheet.
All clocks internally are referenced from the CLIN that directly drives ADC as a sample clock.
The clock divider is a division of the CLKIN prior to or imbedded in the SERDES PLL (not shown in the block diagram).
The clock divider can be set to divide-by-2 or divide-by-4 (Register 53, bit 7)
The SERDES PLL provides a 10x or 20x multiplication (40x mode is not shown in the block diagram). Probably because the divide-by-2 or 4 is inside the SERDES PLL block I am guessing?
For the Mode 0 (LMF = 484 case), the CLKIN frequency max = 500 MHz. In this case, the SERDES bit rate is 10 Gbps.
The PLL mode = 40x. Is the 40x interpreted as the multiply of CLKIN/2 rate to the SERDES bit rate?
Is this interpretation correct? I just want to understand the 40x mode definition from both the JESD mode and JESD PLL mode.
It seems that the actual JESD PLL definition is 20x mode with divide-by-2. What specifically is the 40x mode internally providing?
Thanks,
Troy Robinson