Part Number: ADC32RF45
Hi,
I am using ADC32RF45 in LFMS=82820 mode. I am only using channel A. I am kind of confused with the number of lanes I should be using. in LFMS since L=8 am I supposed to use 8 lanes or 4 lanes? When I implemented a JESD IP core on FPGA side with 4 lanes and checked the ILA configuration data that comes to FPGA from ADC I see number of lanes required for link is 8. When I also cheked the lane IDs of the lanes in use I see numbers 4 to 7. I only connected 4 lanes since I am only using ChA. Am I doing anything wrong? This mode of operation seems confusing to me. If I'd like to use ADC32RF45 CHA only in LFMS=82820 mode should be using all 8 lanes or only 4 lanes?
Erdal