This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC32J45EVM: How does ADC32J45EVM work?

Part Number: ADC32J45EVM
Other Parts Discussed in Thread: DRV10963, DRV10974, ADC32J45

DEARS.

I installed the ADC32J45EVM GUI(ADC3000).
I can not find the "ADC3xJxx_160MSPS_Operation_LMK_Setting.cfg" file in the guide document.
The installed CFG folder contains Config1, Config2.
The contents are as follows.
How does it work?

*Config1*
DRV10963
0x00 0xFFFF
0x00 0x00
0x01 0x00
0x02 0x05
0x03 0x76
0x04 0x00
0x05 0x00
0x06 0x00
0x07 0x0D
0x08 0x00
0x09 0x00
0x0A 0x00
0x0B 0x2E
0x0D 0x09
0x0E 0x00
0x0F 0x81
0x10 0x08
0x11 0x1C
0x12 0x00
0x13 0x90
0x14 0x00
0x15 0x04
0x16 0x00
DRV10973
0x17 0x00
DRV10974
0x01 0x00

*Config2*
DRV10963
0x00 0xFFFF
0x00 0x00
0x01 0x00
0x02 0x05
0x03 0x76
0x04 0x00
0x05 0x00
0x06 0x00
0x07 0x0D
0x08 0x00
0x09 0x00
0x0A 0x00
0x0B 0x2E
0x0D 0x09
0x0E 0x00
0x0F 0x81
0x10 0x08
0x11 0x1C
0x12 0x00
0x13 0x90
0x14 0x00
0x15 0x04
0x16 0x00
DRV10973
0x17 0x00
DRV10974
0x01 0x00

Thank you