Part Number: ADS42JB69
Hi,
I would like to confirm that I can use a sample clock frequency at 160 MHz. And how do I calculate the Max f serdes (table 6 page 34 on the datasheet) ?
Thanks,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS42JB69
Hi,
I would like to confirm that I can use a sample clock frequency at 160 MHz. And how do I calculate the Max f serdes (table 6 page 34 on the datasheet) ?
Thanks,
Hi Daniel
Yes, the ADS42JB69 can support a clock rate of 160 MHz.
At that clock rate the 10x serialization mode must be used with 2 SERDES lanes for ADC A and 2 lanes for ADC B (4 lanes total).
The output data rate will be 10 x 160 = 1.6Gbps on each of the 4 lanes.
Best regards,
Jim B