This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1013: Time from when 0 is written to mode bit until the first conversion ready pulse is output

Expert 8760 points
Part Number: ADS1013


Hi team,

My customer wants to know the time from when 0 is written to mode bit
until the first conversion ready pulse is output.

Please let me know.

Best regards,
Fumio Nakano

  • Hi,


    The amount of time it takes to go into continuous conversion mode can be calculated from the following:

    First, there is a delay of about 20us maximum to allow for the device to start up.

    Second the data rate is a factor in the conversion time. If the data rate is 128SPS, this is about 7.8ms. If the data rate is 3300SPS time is 303us.

    For the nominal (average) conversion time you add the two together. However, for the maximum conversion time, you need to consider the internal oscillator variation. In that case, the data rate variation is ±10%. If you need the maximum conversion time, add 10% to 1/(data rate) for the calculation.


    Joseph Wu
  • Hi Joseph-san,

    Thank you for your prompt reply.
    Your answer is very helpful.
    Thank you!!

    Best regards,
    Fumio Nakano