Part Number: ADS1198
Other Parts Discussed in Thread: ADS1299
Good day,
I would like to use the ADS1198 in a unipolar configuration for a signal that can range between 0 and 5V. To do this I plan to tie all INN at 2.5 and have my input signals on INP and configure the registers for vref = 4V. However while reading the datasheet I am getting the impression of reading two differing pieces of information :
"The analog input to the ADS1198 is fully differential. Assuming PGA = 1, the differential input (INP – INN) can span between –VREF to +VREF."
"When the input is single-ended, the INN input is held at the common-mode voltage, preferably at mid-supply. The INP input swings around the same common voltage and the peak-to-peak amplitude is the (common-mode + 1/2VREF) and the (common-mode – 1/2VREF)."
If I believe the later version I would only be able to mesure tensions from 0.5V to 4.5V for a common mode of 2.5V. Am I understanding this correctly ? If so how can I use this device for the above specified need ?