This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS42JB69: Need Clarification Interpreting Datasheet

Part Number: ADS42JB69


Hi,

This is the part that I am not sure:

"The input common-mode is set internally using a 5-kΩ resistor from each input pin to VCM so the input signal
can be ac-coupled to the pins."

Does this mean I have to put an external resistor in series from VCM to each leg?

Does it mean I don't have to worry about external resistor because they are all internally connected?

I know it is a basic question but I really need clarification.

Thanks.