Part Number: PGA900
I've read through the data sheet for the PGA900 and have tired to figure out how to estimate its power consumption. I'd like to confirm my approach to estimation since there is no direct info on this in the data sheet that i can find.
I am interested in getting a rough estimate for it working with two wheatstone bridge based pressure transducers. At the moment, the details of those transducers is not set so I can't say what the base resistance will be --- I am using a typical gage value of 1000ohm for now (350 is common as well).
This estimate is important in my application because I am looking to run this off a battery and I need get a rough sizing estimate for a week's operation time.
Section 6.3 for the data sheet says the max current in normal operation is 2.5mA -- that is without excitation of the bridge. I am expecting to supply the chip with 3.3V from a voltage regulated LiOn battery.
Section 6.10 says that typical bridge excitation voltage is 2.5V and typical current supply to bridge is 1.5mA. This current draw seems at least somewhat consistent for 1000 ohm bridges.
Using the above, I get 8.25mW for the chip plus an additional 3.75mW for the bridge. I am running two bridges so 7.5mW for them. Meaning an overall power consumption of 16.25mW
Does this estimate sound right?